Cancel
Showing results for 
Search instead for 
Did you mean: 

AutoCAD Import Paperspace scale

Not applicable

Hi all
Importing a Autocad drawing with model to scale in model space
and 2 sheets.
All the dimensions etc have been added on the sheet and include an appropriate
scale factor in the propertires (0.01) i.e. the paper view is 1/10 the model
when i import to SolidEdge V20 everything works except the dimensions have lost
their scaling info
so a dimonsion that should read 1115 now reads 111.5
so it appears that the paper space has been scaled correctly but the dimensions
are reporting the scaled dimension
any clues ?
thanks
Donald
2 REPLIES 2

Re: AutoCAD Import Paperspace scale

Not applicable
Donald,
Can you provide a simple example. I created a simple AutoCAD example and
translated it into Solid Edge. I had a viewport on Layout1 that referenced
the geometry on the Model. I set the scale of the viewport to .5. I placed a
dimension on the line in the viewport on Layout1. I translated the file into
Solid Edge and the dimension was the same. Is this the correct workflow?
Regards,
Rick B.

Re: AutoCAD Import Paperspace scale

Not applicable

Ricky,
Thanks for the reponse, I am now completly confused
Your interpretation of the workflow is correct
I repeated your simple excercise and the conversion worked
I took the existing drawing
created a new viewport placed one dimension and imported
again the SolidEdge reports the actual dimension of the line in the paper space
rather the correct scaled dimension.
however if i place a dimension using SolidEdge it reports the correct scaled dimesion
Thanks
Donald
"Ricky Black" wrote:
>Donald,
>Can you provide a simple example. I created a simple AutoCAD example and
>translated it into Solid Edge. I had a viewport on Layout1 that referenced
>
>the geometry on the Model. I set the scale of the viewport to .5. I placed
>a
>dimension on the line in the viewport on Layout1. I translated the file into
>
>Solid Edge and the dimension was the same. Is this the correct workflow?
>
>Regards,
>Rick B.
>
>