Cancel
Showing results for 
Search instead for 
Did you mean: 

Autocad Sketch to Solid Edge Paste??

Pioneer
Pioneer

Hello
The existing Solid Edge Solid Edge Sketch sketch version in Autocad environment
Copy-pastes were impossible.
The ST8 version is that the paste to the Edge Sketch environment in Autocad Skech
I want to make.
Can you confirm?

2 REPLIES

Re: Autocad Sketch to Solid Edge Paste??

Gears Phenom Gears Phenom
Gears Phenom

AutoCAD sketch can be copy pasted directly into Solid Edge though not in the Sketcher.

I don't believe people involved in ST 8 beta would be allowed to reveal this.

But since you are asking, that is a scoop.

Re: Autocad Sketch to Solid Edge Paste??

Legend
Legend

Will it work in 3D?

Using SE since V12, 2002
ST10 certified