Cancel
Showing results for 
Search instead for 
Did you mean: 

Automated Design

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I am automating an assembly in excel, so far I have had it change the number of parts by changing my length and width. What I would like to do is change out a subassembly with another subassembly just being driven by excel. I have been able to do it with alternate assemblies but i cant find a way to control that with my excel file. Is there a way to drive my alternate assemblies with excel or should I be looking in another direction to change a subassembly through excel?

3 REPLIES 3

Re: Automated Design

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@alexhurd  If you do not wish to use the Alternate Assembly functionality, you should still be able to change out components but you would need to do this using VB code in Excel (Macros) and would need to do this with the Solid Edge API (Appplication Programming Interface).



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Automated Design

Gears Phenom Gears Phenom
Gears Phenom

@alexhurd  you may have more luck posting automation question to the SE Developer's Forum

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Automated Design

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thank you Matt I just reposted