Cancel
Showing results for 
Search instead for 
Did you mean: 

Automatic centerlines does not work on broken section-view?

Valued Contributor
Valued Contributor

Hi,

 

I have tried to use "Automatic Centerlines" to a section-view that has been shortened using "Add Break Lines", but failed so far.

 

Is it possible to automatically add centerlines to a broken section-view?

 

 

 

Regards,

 

Kenneth

2 REPLIES

Re: Automatic centerlines does not work on broken section-view?

Valued Contributor
Valued Contributor

I am currently on ST5, and what you have to do is add the centerline before you add the break lines.  Then it should work.

 

Re: Automatic centerlines does not work on broken section-view?

Honored Contributor
Honored Contributor

Auto center line also don't work when the center of the hole is outside a flat pattern.

It would be nice if you could add just one that stays with the view. The manual ones don't stay with the view when moved. I end us using the Auto, and delete the ones I don't want. Bad work flow.