Cancel
Showing results for 
Search instead for 
Did you mean: 

Autosave, automatic save files in solid edge

Pioneer
Pioneer

I want to set up automatic save option in solid edge st7, I went to solid edge option ...save...click on auto save and setup time (see image) but after that much of time it asked me a question, do you want to save it? I want it automatically done not manually. Can anyone help me with this?

 

1 REPLY 1

Re: Autosave, automatic save files in solid edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That is how the Solid Edge AutoSave works.  At the selected interval, it waits till the active command is complete and then prompts you to Save.

 

If you are doing this in case of a crash, you may want to use the Auto Backup Copy which is fully automatic.  Just make sure you read the help about it first so that in the event of a crash, you know how to properly restore the file.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com