Cancel
Showing results for 
Search instead for 
Did you mean: 

BOM reports

Creator
Creator

 I have an adjustable part in an assembly. When I run the report the quantity for that part is EA. Is there a way to have adjustable parts show as inches?

3 REPLIES 3

Betreff: BOM reports

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JustinMc 

 

 

not sure what "EA" is, but if th eadjustable part is seen as soemthing like a frame, a profile, a cable, etc. and You need the correct length of every piece, then I would suggest to either use the structure frame functionallity or as talked in another post today morning with user defined quantities and user defined quantity units.

 

 

regards
Wolfgang

Betreff: BOM reports

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JustinMc 

 

 

 

here is the link to the article/post I have talked before:

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Extra-bolt-quantity-in-assembly-BOM...

 

 

regards
Wolfgang

Re: BOM reports

Legend
Legend
Instead of using the unistrut as an adjustable part instead make it a frame structure component so you can use the BOM tool to give you the lengths you desire.