Cancel
Showing results for 
Search instead for 
Did you mean: 

Barc code font changes when saving as DWG

Pioneer
Pioneer

Hi all,

 

On all machines, after ST6 MP8 release, we have started facing font changing problem when saving as .DWG

 

We are using "Free 3 of 9" Font for writing barcodes on .dft files, but when saving as .DWG or .dxf (!after MP8 release!) font changes to a normal letters font. Only .PDF have no problem.

 

Attaching pictures fo better understanding:

 

how dft look:

dft.jpg

 

.DWG before upgrade

2.jpg

 

.DWG after MP8

3.jpg

 

Please help ! Smiley Happy)

4 REPLIES

Re: Barc code font changes when saving as DWG

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Are the DWG/DXF being open on the same PC?  If so, it is probably the font mapping options when you save them out of SE.  Check your Options when you go to save out a DXF/DWG and on the font mapping page set the map correctly for the barcode font you are using.

 

If it is a different machine, insure the font is installed on the machine opening the DXF/DWG.  PDF's can embed fonts so if the destination PC doesn't have them, they still work.  Most other files do not, including DXF/DWG so the fonts have to also be installed wherever the DWG/DXF files are opened.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com

Re: Barc code font changes when saving as DWG

Pioneer
Pioneer

Hi Grundey,

 

Just before update MP8, everything worked perfectly, so font missing problem is not the problem.

I want to specify, that before installing MP8 i had only MP4 update.

it so big problem.. :/

Re: Barc code font changes when saving as DWG

Pioneer
Pioneer

Which files are responsible for dft/DWG/dxf convertation ? We would like to replace those files from clear, not updated copy of solid edge.. 

Re: Barc code font changes when saving as DWG

Pioneer
Pioneer

Find a solution! Smiley Happy

 

Yes, after update, font dissapeared from autocad font list, so wee added the font again from drop down list, but you need to rename the same name autocad font on the left side.

 

Few pictures if anyone else will face this problem Smiley Happy

 

1a.jpg 

1b.jpg