Cancel
Showing results for 
Search instead for 
Did you mean: 

Basic 3D sketch dimension

Valued Contributor
Valued Contributor

Hi,

 

Why can't i center the box?

I'm not able to dimension from center to edge of box... no idea why.

 

12 REPLIES 12

Re: Basic 3D sketch dimension

Gears Phenom Gears Phenom
Gears Phenom

looks like you are picking the Csys point and not the Axis...   thus I believe the dimension is inferring min distance measurement.  try the SHIFT key to toggle to Horz/Vert  and/or  pick the Axis and not the point

 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Basic 3D sketch dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Kenneth,

 

Further to what @Johnson_BigMatt points out....you could also use relationships to locate the geometry to.....say, use  "Connect" at line mid point to the relative Csys axis.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Basic 3D sketch dimension

Honored Contributor
Honored Contributor

Try starting the dimension from the origin planes as the first step.

Re: Basic 3D sketch dimension

Valued Contributor
Valued Contributor

I used connect to fix the issue, but already got the same problem again Smiley Sad

 

What am I doing wrong? Trying to align the 2 lines to each side of center. Can't even dimension the distance to center, as you can see in the video.

 

I try to select the plane/line instead of the center-dot. Still no success.

 

Hope one of you might be able to help me Smiley Happy

 

 

Re: Basic 3D sketch dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Kenneth

 

 

You will be successfull when activating the "Lock Dimension Plane" button for 3D sketch dimensions

 

See video.

 

(view in My Videos)

 

before locking the plane the dimension behaves the same as Yours, but after acitvating the lock plane it is at You expect it to be.

 

regards
Wolfgang

Re: Basic 3D sketch dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Oh man @hawcad, you are soo fast.......I was just writing about that very thing, untill I saw the email notification for your answer.  Robot Happy

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Basic 3D sketch dimension

Valued Contributor
Valued Contributor

Awesome, thanks!

Re: Basic 3D sketch dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What is "automatic" in the dim dropdown? Is that an ST10 thing or am I losing my mind?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Basic 3D sketch dimension

Valued Contributor
Valued Contributor

Think it was in ST9 too