Cancel
Showing results for 
Search instead for 
Did you mean: 

Batch Print Option

Experimenter
Experimenter

Hi,

I am a SE 9 user & want to use batch.exe from location:

C:\Program Files\Solid Edge ST9\Custom\Batch\Bin

to covert all dft files to pdf with their file name & title of the associated par file (Example: 123456-001_MANIFOLD).

Please let me know if we can set it somwhere to do this default  type OR any macro required to do this.

 

Thanks,

Shivraj

19 REPLIES

Re: Batch Print Option

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I have customised the Batch.exe several times in the past to add new features.

Batch.exe does not appear to support 2D PDF in its current state, I could not find this in the list of options.

 

BatchPDF.png

 

Also did not understand "with their file name & title of the associated par file"

 

~Tushar

 

Re: Batch Print Option

Phenom
Phenom

@Tushar Is .PDF not directly above the 3D PDF you have highlighted? I use this standard batch program to create drawing PDF's all the time.

 

I think the OP wanted to include additional information in the PDF filename and that is not possible with the standard batch file as far as I know. It simply saves out as the same name as the draft file.

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Batch Print Option

Experimenter
Experimenter

Thanks Tushar for reply.

I would like to convert the file to pdf through Batch where you can find the option with name Adobe (*.pdf) this covnverts the dft to 2D pdf.

 

Now if I have a dft file with name 123456-001.  Same is created with one par file whose Title in the Fileproperty is written as MANIFOLD then the pdf file to be saved as 123456-001_MANIFOLD

 

Hope this clarifies.

Thanks,

Shivraj

Re: Batch Print Option

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Pampac, @rehenryjr, @Tushar

 

 

I believe,  that I have done an adabtion to my SE-Export macro to use the same  file naming conventions for filename and foldername, but based onto the batch macro. 

 

Maybe it must believhave modified and be translated ontologisch English. 

 

I will keep You informed. 

 

 

regards
Wolfgang

Re: Batch Print Option

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Oops. It was hiding in plain sight, just above the item selected in my screenshot.

 

@Pampac would it be ok if I write a macro to change the draft file names to append the Title property from its related part file, so you could still use the batch.exe to export a PDF?

 

I think then this will require an antidote program to change the draft file names to its original  ones; or alternatively copy the drafts to a new folder where they could be renamed using my macro.

 

Though I would prefer waiting for an adaptation of Worlfgang's macro since it already exists.

 

Re: Batch Print Option

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Tushar

 

 

 

using the batch macro fro printing to PDF would need an extra PDF printer or an adaption to use a save as PDF from draft

 

As mentioned, I believe that I have done this a couple of years ago - just have to search for it.

 

 

regards
Wolfgang

Re: Batch Print Option

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Yes. As I agree, it would be better to use something already available than writing a new macro.

Re: Batch Print Option

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Tushar

Hi @Pampac

Hi @rehenryjr

 

 

 

and - sometimes I wonder about myself - I have found the modified batch macro, and it already was set to be used in English or German and so I can put it here as attachment in English

 

Please - ATTENTION - take first a look into the INI file.

There nearly evrything can and must be defined.

This means, You can define

 

  • where (folder) the PDFs should come into.
    This can be an absolute path or a realtive to the draft file folder
  • what the PDF filename should be

For both definitions You can use any property text from the draft file, using the typical SE proeprty call out syntax like
%{propertyname}

During the macro execution I replace any of these placeholders by the appropriate text

 

Please keep in mind that for the filename itself only the German verb %{Dateiname} is used, as well as for Time, which is %{Zeit} and Date which is %{Datum}

This is thought for adding the time and date of printing to the filename for differ between different versions and printouts.

 

 

All the other options are set by certain numbers/values which are explained within the INI file in German as well as English.

So please take a short look into.

 

If there are any questions, don't hesitate to aske me via the forum or via personal mail

 

Hope it helps

 

PS.: the INI  syntax is the same as for the single version SE-Export

 

PS2.: You can save PDF as well as DXF from draft or even both at the same time

 

 

regards
Wolfgang

Re: Batch Print Option

PLM World Member Genius PLM World Member Genius
PLM World Member Genius
Hi Wolfgang,
I use SE-Export almost every day it is handy and very useful. May I ask you if you could write a similar program for exporting step. files. Currently I use Batch.exe but would be better to be able to export step file automatically from an open file.
Thank you,
Marc