Cancel
Showing results for 
Search instead for 
Did you mean: 

Batch (bulk) edit file properties

Experimenter
Experimenter

Hello all,

Problem : I have hundreds of file that I have to edit the same field in the ''Custom File Properties''.

One way to go is to open each file manually, go into ''File Properties'', go to ''Custom'' tab, click on the field that needs editing, edit it, save, close and repeat.

Is there a way to select all files (all parts) and change, all at once, a field in the custom ''File properties'' ?

Or any other application to batch (bulk) edit .par/.psm files ?

Thank you,

Sam

4 REPLIES 4

Re: Batch (bulk) edit file properties

Gears Phenom Gears Phenom
Gears Phenom

yes,  Property manager .

 

Does exactly that.

 

you can edit all props from an assembly structure

or for all files in a folder location.

 

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Betreff: Batch (bulk) edit file properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Vendetti1000

 

 

 

as @Johnson_BigMatt already said (YOu were faster) the Proeprty Manager exactly will do this for YOu and will help You.

 

You can use it from explorer too and You will not need to open a SE file before.

 

Make it proper for first (that menas, let it show all proeprties You want) and then You can use it.

 

 

regards
Wolfgang

Betreff: Batch (bulk) edit file properties

Valued Contributor
Valued Contributor
How do I use property manager on a number of draft files to change title block properties (custom)? I cant see how to start it in Explorer.

Thanks,
Guy

CAD/CAE Manager
SE2019 MP5

Betreff: Batch (bulk) edit file properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

With nothing open in SE go to the info tab in the application button, pick property manager, select the files you want to work on.

Or you can get to the same place in Design Manager which has a property manager under the app button.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200