Cancel
Showing results for 
Search instead for 
Did you mean: 

Batch or Auto Update

Valued Contributor
Valued Contributor

Is there a Solid Edge feature to automaticaly update on open or maybe batch update draft views instead of opening each individual draft file and manually pressing the update button?

 

If I remember correctly, Solidworks used to have a batch option that would open, update, and close models and drawing files.

 

Thanks,

 

Matt

4 REPLIES 4

Re: Batch or Auto Update

Siemens Phenom Siemens Phenom
Siemens Phenom

Look at the OpenSave macro in the C:\Program Files\Solid Edge ST8\Custom\OpenSave\bin folder.

 

There is an option to open draft files and update views:

 

opensave_draft.png

Highlighted

Re: Batch or Auto Update

Valued Contributor
Valued Contributor

Thanks.

 

Matt

Re: Batch or Auto Update

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
 
smitsch@unitec.de
www.all4edge.de

Re: Batch or Auto Update

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Very good idea!

Will work for the visible thin grey frame around the views.

 

For the problem with the thick corners you will need to have a third party solution.

 

I know only one solution "SeDftUpdate".

This solution will follow all links and will update them and the views in the draft.

 

Works interactively but most of the user make use of the batch run. The update process runs in the background or over night.

 

Stefan

 

 

 

smitsch@unitec.de
www.all4edge.de