Cancel
Showing results for 
Search instead for 
Did you mean: 

Beam element frame analysis

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Hi All,

 

I'm currently working on an FEA for a frame (sketched up with the frames command). The trouble I am having is that all the elements are not joining together in the model as shown in the picture below

 

Capture.PNG

In some areas it adds a connector like this automatically

Capture.PNG

Is there anyway I can add that in a manual fashion?

 

 

Shane Murray
SE2019 MP3
2 REPLIES 2

Re: Beam element frame analysis

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I don't think there is a manual way to add a connection at that point.

What you need to make sure is that your sketch support lines do connect.

Re: Beam element frame analysis

Siemens Phenom Siemens Phenom
Siemens Phenom

As FredMenage replies, there is no manual way to connect these elements. 

 

Be sure they are connected in the Frame sketch and if still not generating connected elements in the Study, log an IR with your support.

 

Good luck!

 

/Ulf

Siemens EMEA GTAC Support