Cancel
Showing results for 
Search instead for 
Did you mean: 

Beginner needs help

Experimenter
Experimenter

Hello guys,

 

I want to make a pyramid with 4 sides and a flat top 

measurements are: length 20cm height 9cm Length top 10cm Corners 60 Degree

 

I tried it with extrusion form oblique but the top always gets a tip

7 REPLIES

Re: Beginner needs help

Experimenter
Experimenter
The name of the figure is called frustum

Re: Beginner needs help

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @Lipton212

 

Don't have an exact solution, but here's a little video to help you get started:

 

 

Hope you find it useful.

 

Tushar

 

Betreff: Beginner needs help

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Lipton212

 

 

if I understand Your request correctly then this is a simple protrusion with an additional  "Draft Treatment Step" 

 

 

See those 2 pictures for explanantion

 

20170603_1756.PNG20170603_1757.PNG

 

 

The only I don't understand as explaned is that with Your request for bottom length of 20, a height of 9 and slope of 60 deg You can not get the top length of 10

regards
Wolfgang

Betreff: Beginner needs help

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Lipton212

 

 

 

and You also can solve Your request by using sync modeling or a traditional Loft feature with two sketches at zero and 90mm

20170603_1804.PNG20170603_1806.PNG20170603_1807.PNG

regards
Wolfgang

Betreff: Beginner needs help

Experimenter
Experimenter

Thanks 

 

I got it now perfect

Betreff: Beginner needs help

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Lipton212

 

 

fine, happy that it got solved finally.

 

And is it possible to fullfill all Your requests?

That means base length 200, top length 100, height 90 and angle 60 degrees?

 

This would be very interesting.

 

regards
Wolfgang

Betreff: Beginner needs help

Gears Phenom Gears Phenom
Gears Phenom

@Lipton212,  For the sake of all in the community...  Please consider giving KUDOS to answers that were helpful to you or appreciated.  Also please mark a post as the SOLUTION if you feel you received an answer.  This helps give credit and creditability to other users and helps others find solution in the future when searching the forums.

 

thanks!

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7