Cancel
Showing results for 
Search instead for 
Did you mean: 

Bending lines and additional text up / down

Legend
Legend

Is it possible to generate drawing views of flat(s) and get additional text f.i. up /down near the bendlines.

At this moment we show the UP line as tangent and the down line as hidden.

 

See attached example

2 REPLIES

Re: Bending lines and additional text up / down

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Yes, you can do this with Bend table or Callout!

 

Here is a video:

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Bending lines and additional text up / down

Legend
Legend

I just setup a formula in my callout box, and point to brake lines with the following:

 

%BO %BN@%BR

 

this will produce <Bend Direction><Bend Angle>@<Bend Radius>

ST8 MP9
Go FAST, or go home.