Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Best Operating System

Gears Phenom Gears Phenom
Gears Phenom

That's really a dang shame with that GeForce 1060, such a great card, just not proper for CAD applications. I have one at home on my VR machine, just seems like that sort of card should be able to support CAD applications. But they have different purposes I suppose.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Best Operating System

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @nominus38

 

 

 

probably it is not a matter of the card as more a question of the proper driver and what the developers are allowing and what not. In that case the developers of the graphics driver.

 

But I agree with You that if the hardware is nearly the same it also should act nearly the same as so called high end graphic cards.

 

regards
Wolfgang