Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Bill of Material Word Wrap

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

If the table margins are set to zero, you might just be able to squeeze in the text on two lines, still complying to company standards.

Re: Bill of Material Word Wrap

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Tushar, I couldn't get any margin settings to make a difference. What setting do you refer to?

@David_McMahonYou may need to loosen the requirement a little if possible. I wonder if this .156/.50 spec isn't a legacy from the manual drafting era? It seems that often people end up working for the spec instead of the spec working for them.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200
Highlighted

Re: Bill of Material Word Wrap

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@bshand

Actually a very little compromise on the standards:

.156/.51 instead of .156/.50

will work, with margins set to 0.