Black PDF Bug?

Valued Contributor
Valued Contributor

I am getting weird black PDF files when I Save As Translated to a PDF file. I think I have isolated the problem to the following:

 

1) The drawing has colored text in the background title block

2) The drawing has dimensioned sketch geometry

3) The PDF options are set to save as color (see below)

 

 

Can anyone reproduce this? See attached draft file.

 

 

black_pdf.png

 

black_pdf_draft.png

 

save_as_pdf_options.png

David McMahon
Solid Edge ST10, MP3
HP Z2 Mini, Windows 10
6 REPLIES

Re: Black PDF Bug?

Siemens Phenom Siemens Phenom
Siemens Phenom

Should be fixed in ST9 MP4.

Re: Black PDF Bug?

Esteemed Contributor
Esteemed Contributor

Hi @David_McMahon

 

 

in the meantime You can change the dimension color from Autocad Black/White to Black (or whatever color You want).

Doing so You can print Your drafts to PDF without any problem.

 

And as mentioned by Dave, it will be fixed with MP4

 



regards
Wolfgang

Re: Black PDF Bug?

Valued Contributor
Valued Contributor

Great, thanks for the confirmation and notice of MP4 fix.

David McMahon
Solid Edge ST10, MP3
HP Z2 Mini, Windows 10

Re: Black PDF Bug?

Legend
Legend

"Save all colors as black" should fix it until MP4 is available.

Greetings from Germany
Christian Kunkel
https://c-k-m.info

Re: Black PDF Bug?

Genius
Genius

Until MP4 will be avilable you can use "PDF Creator" aplication.

SE ST9 + TC 10.1.7

Re: Black PDF Bug?

Genius
Genius

I'm getting the same problem printing to our A1 plotter, Robot Sad