Cancel
Showing results for 
Search instead for 
Did you mean: 

Block Libraries

Not applicable

Hi all.
I was wondering if anyone knows whether solid edge has any additional block/symbol
libraries that can be downloaded. The ones that came with the programme are pretty
limited. I know that objects can be drawn and then added to the libraries, but if
there are already other libraries out there that can be downloaded and used, why
reinvent the wheel.
Thanks
John
1 REPLY 1

Re: Block Libraries

Not applicable
Solid Edge does not have additional block libraries that I know of. I think
the intent was to be able to get the commercially available AutoCAD block
libraries and convert them (see Help).
--
Ken
http://grundey.blogspot.com
"John" wrote in message
news:48d8a950$1@bbsnotes.ugs.com...
>
> Hi all.
>
> I was wondering if anyone knows whether solid edge has any additional
> block/symbol
> libraries that can be downloaded. The ones that came with the programme
> are pretty
> limited. I know that objects can be drawn and then added to the libraries,
> but if
> there are already other libraries out there that can be downloaded and
> used, why
> reinvent the wheel.
>
> Thanks
> John