Cancel
Showing results for 
Search instead for 
Did you mean: 

Break Lines Dimension change.

Experimenter
Experimenter

Howdy all,

I have a problem with a dimension i changing after break lines have been applied. Is there a way to fix the dimension without manually changing the dimension to blank and typing in the correct dimesion? Attached are snap shots of my problem.

 

 

 

8 REPLIES 8

Re: Break Lines Dimension change.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The problem you are having is not clear in the two jpegs.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Break Lines Dimension change.

Experimenter
Experimenter
The 1/4" dimension, shown at item 12, changes to 1/2" after I apply the break.

Re: Break Lines Dimension change.

Gears Phenom Gears Phenom
Gears Phenom

That is funky. I have it where the attachment points of the dimension overlap the part edges when I apply a break, but I've NEVER seen it change the readout of the dimension. What happens if you add the dimension after you apply the break?

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Break Lines Dimension change.

Experimenter
Experimenter
I tried both ways and the result is the same.

Re: Break Lines Dimension change.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That is odd since it doesn't seem to be involved in the break at all.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Break Lines Dimension change.

Experimenter
Experimenter
I managed to fix the problem. For some reason Solid Edge didn't like the way I defined the configuration that I was using to show the detail. I created a new sub-assembly and recreated the view, and the problem fixed itself.

Re: Break Lines Dimension change.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

 

I am on the same boat and have seen similar issue.

 

Could you please point me in the right direction on how you fixed this issue by changing configuration. Where can I find show details in configuration?

 

I want to see if I could solve this problem the same way as you did?

 

Thanks in advance.

Re: Break Lines Dimension change.

Experimenter
Experimenter

I had to create a sub assembly of the parts, and then create a configuration in my top level assembly. In my draft I then selected the new configuration to be displayed. My company uses a lot of configurations which is why I did it this way, but it is not nessicarily the best way.