Cancel
Showing results for 
Search instead for 
Did you mean: 

Bug in 'Copy to Library' - draft

Dear fellow Edgers,

I have found a bug in the draft enviroment and would like to ask you if you could try the following and see if there it is a general bug or something only on our workstations.

 

  1. Make a simpel text like hello or something.
  2. Make sure you have more text fields in the draft and/or tables.
  3. Select the 'Copy to Library' tool and select 1 text field.
  4. After the safe of the Library text, open the file and see if there are multible text fields or tables in it.

I have tried it multible times, even after a complete new install of SE and I see multible text fields in the library draft than the one that I have selected.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10
6 REPLIES

Re: Bug in 'Copy to Library' - draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Daniël,

 

Nope....not seeing this issue, only getting the single entry, as saved.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Bug in 'Copy to Library' - draft

Weird...

Thank you for the test
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Bug in 'Copy to Library' - draft

Gears Phenom Gears Phenom
Gears Phenom

I am on ST6.

No issues found.

 

~Tushar

 

Re: Bug in 'Copy to Library' - draft

Does anyone know what might be the cause of this strange behavior?
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Bug in 'Copy to Library' - draft

Gears Phenom Gears Phenom
Gears Phenom

What are those other zoombie objects like - selectable or just graphic impressions ?

In case of later, could be just a graphics issue.

If real objects, then a quite serious problem Robot surprised

 

~Tushar

 

Re: Bug in 'Copy to Library' - draft

These objects are some zombie objects but also real objects.
Even already objects that have been placed from the library and placed as blocks.
I will upload a draft with some blocks and one text for to transport to the library, perhaps it is a draft template error from our side.

I have tried to send the text field on the top-left side to the library.

 

I have uploaded 4 drafts with no models placed.

The 'Test draft' and _AA-Test are tested after each other. The 'Test draft2' and __BB-test after eacht other.

 

Please check if it's our error or a general error.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10