Cancel
Showing results for 
Search instead for 
Did you mean: 

CAN'T CLOSE INDIVIDUAL FILES

Genius
Genius

I now have "that" new computer with Windows 10.  I find that when I have multiple ST8 files open at one time, there is no option to just shut one. It's either all or none.

 

Thanks,

Ron

2 REPLIES

Re: CAN'T CLOSE INDIVIDUAL FILES

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Ron,

 

One way [and there is a BETTER solution on the horizon, with ST9] is to minimise the documents, so you can identify them for selected activating, or in your case, closing.

 

ST8_PAR_MultiDocumentView.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Re: CAN'T CLOSE INDIVIDUAL FILES

Genius
Genius

Sean, it took me some time to figure out just why I experienced this problem.  And I discovered the reason accidentally.  I had chosen SIVER as the APPLICATION COLOR SCHEME under SE OPTIONS/HELPERS. In this configuration, the MIN/MAX/CLOSE icons in the upper right hand corner that affect the individual files (not the overall software)  are a  pale yellow and nearly invisible.  When I realized this, I went back and checked my records.   I had previously used what is now called (and may've always been called) CLASSIC SILVER.  In this scheme, the above icons are clearly visible.

 

For whatever it may be worth to others.

 

Thanks,

Ron