Cancel
Showing results for 
Search instead for 
Did you mean: 

CATIA Interface

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


we have tested the CATIA V5 Translator.

 

Import of CATIA files sems to be o.k so far, but export a Solid Edge document to CATIA results in an opening error by CATIA.

 

As I have understood, the export files should be V5 R14 and therefore should be readable by R19 or higher, isn't it?

 

Since we only can send export files for testing but can not open them by ourself, please

can anybody confirm, wether or not a Solid Edge exported CATIA file will be possible for opening in CATIA

 

Thanks and

 



regards
Wolfgang
4 REPLIES

Re: CATIA Interface

Gears Phenom Gears Phenom
Gears Phenom

Hi Wolfgang:

 

What is your SE version?

ST 6 supports readily up to R22.

But there are too few options to control in the SaveAs dialog.

See this matrix for CATIA V5

 

~Tushar

Re: CATIA Interface

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Tushar,

 

 

 

the test was done with ST7.

 

I can repeat it with ST8 too.

 

 



regards
Wolfgang

Re: CATIA Interface

Gears Phenom Gears Phenom
Gears Phenom

Hi Wolfgang:

 

Can you post a sample CATIA file exported from ST7.

I can test it with V5 R17 if that helps you.

  

~Tushar

Re: CATIA Interface

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

thanks for assisting and I will post an example on Monday

 

 



regards
Wolfgang