Cancel
Showing results for 
Search instead for 
Did you mean: 

CHANGE ANGLE OF SURFACES IN SE ST9

Pioneer
Pioneer

I want to change angle of surfaces to +/- 1 deg. The surfaces have green/orange colour as in the picture below.

before.PNG

 After the changing I want to have something like below.

 

after.PNG

3D model in attachment. If it possible please create movie step by step to do it.

 

Thanks.

I did, I understand.
4 REPLIES

Betreff: CHANGE ANGLE OF SURFACES IN SE ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Father

 

 

 

 

first I thought what a simple question, this just is either a draft surface or since YOu already have replacement surfaces there, a Surface Replace feature.

 

But both of them didn't work.

 

Wow!

Why?

 

After inspecting Your part I have seen that there is a problem surface (cylinder R9) which goes downwards into the model area.

So I first also trimmed this surface back to the plane

 

 

Then export as STEP and reimport with all healing options on, moving the part and optimize the model

 

And now a simple Draft with Split option ons did the job.

 

See video and finished part.

Attention: draft angle might not be 1 degree just to see the draft angle better in the model

 

 

 

regards
Wolfgang

Betreff: CHANGE ANGLE OF SURFACES IN SE ST9

Pioneer
Pioneer

@hawcad thanks a lot for your help Man Happy

I did, I understand.

Betreff: CHANGE ANGLE OF SURFACES IN SE ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Father

 

 

 

welcome, is it as You wanted it?

regards
Wolfgang

Betreff: CHANGE ANGLE OF SURFACES IN SE ST9

Pioneer
Pioneer

@hawcad is OK. I have expected this solution.

 

Thanks.

I did, I understand.