Cancel
Showing results for 
Search instead for 
Did you mean: 

CLONE LOGO COMPANY AFTER EXPORT DWG

Pioneer
Pioneer

Hi,

 

someone help me about a problem after I export a file draft in .dwg.?

When I export a .draft in .dwg, automarically, a .jpg file of the company logo will apper in the same saving location as the .dwg file.  This happens every time you save, a jpg file is creatend and the namefile is the namefile of the .dwg. 

It seems a link...but I won't it.

Thank you in advance

Capture.JPG

 

 

 The icon up, is the .jpg (logo company) created after export in dwg the draft.

5 REPLIES 5

Re: CLONE LOGO COMPANY AFTER EXPORT DWG

Legend
Legend

Hello @UtAgr,

 

You pasted the logo inside your draft, mostlikely with CTRL+V.

 

When you make a snip of that logo you have at top left under "Home" the option "Paste Special". When you do it through that you won't get the file when making DWG.

 

 

Sander
The Netherlands
Highlighted

Re: CLONE LOGO COMPANY AFTER EXPORT DWG

Pioneer
Pioneer

Thank you Sander,

I've try your trick and it works. But I don't think this is the right way.
I know that it's possible to inseCattura.JPGrt a bitmap/jpg/png file by the button that you see below (by arrows)

 

 

 

 

 

So, at the moment I'm using your method but someone can can deepen the topic.

Thank you 

Re: CLONE LOGO COMPANY AFTER EXPORT DWG

Gears Phenom Gears Phenom
Gears Phenom

Depending on your export needs, single file or multiple, you can select the options on the export page.

 

dwg options.jpg

-Craig

Re: CLONE LOGO COMPANY AFTER EXPORT DWG

Pioneer
Pioneer
Not work. Why the solution should be given by how I export to dwg? What you say refers to when there are more drawing sheets to be exported. It is possible to export all the drawing tables in a single file or in several different files, although at least one copy of the company logo image is created. Why?

Re: CLONE LOGO COMPANY AFTER EXPORT DWG

Gears Phenom Gears Phenom
Gears Phenom

I would encourage you to convert the logo into arc, circle and lines.

The result it will be much better and no links to file must be created.

 

There is also some free online tools to convert from image to vector