COMO TRANSFORMAR UM SURFACING EM SÓLIDO?

Experimenter
Experimenter

COMO TRANSFORMAR UM SURFACING EM SÓLIDO?

2 REPLIES

Hi there,   You would need to make sure the surfaces crea...

Esteemed Contributor
Esteemed Contributor

Hi there,

 

You would need to make sure the surfaces create an fully enclosed "volume"....then using the "Stitch" command should make it a solid model.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

It has been a while since I did this, but I think once al...

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

It has been a while since I did this, but I think once all the surfaces have been stitched together to make a "water tight" volume, Solid Edge will ask if you want to make it a solid feature.

 

There are also methods of using Boolean and Thicken to create solids from surfaces.


____________________________________
--Scott Wertel, P.E.