Cancel
Showing results for 
Search instead for 
Did you mean: 

CUT EXTRUDED BODY

Experimenter
Experimenter

Hi,

 

I am having issues cutting/cut revolving an extruded body of part. the part is not in construction state.

The cut will preview, but thats as far as it gets. Im thinking it maybe a software problem.

using the hole command it will cut.

Can anyone see any reason why this would not work?

 

Thanks Ian

 

 

17 REPLIES

Re: CUT EXTRUDED BODY

Gears Phenom Gears Phenom
Gears Phenom

@ian876

Hi,

Could you upload your model please to see what is going on?

Regards,

Arek

Re: CUT EXTRUDED BODY

Experimenter
Experimenter

Hi Arek,

 

this is happening to all models and even when i create a new part.

 

thanks

Re: CUT EXTRUDED BODY

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Sometimes this happens when you key in a distance, the preview will show and you need to click again to set the direction.

 

If that is not it, then you will need to take a video of the process and post it so we can see what is going on.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: CUT EXTRUDED BODY

Experimenter
Experimenter

(view in My Videos)
This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

Re: CUT EXTRUDED BODY

Gears Phenom Gears Phenom
Gears Phenom

Are u able to log into this PC as another user and retest?   this is quite odd.

 

Also what Version and MP are you running.

 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: CUT EXTRUDED BODY

Experimenter
Experimenter

when i log on as another user it works as normal.

seems specific to my user.

 

many thanks

Re: CUT EXTRUDED BODY

Experimenter
Experimenter

and its ST9

Re: CUT EXTRUDED BODY

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @ian876

 

 

then it seems as Your Current User "Profile" (registry) is corrupted somehow.

 

I would do a reset to default with deleting the Current User Regiostry of Solid Edge v109

 

PS.: for such situations I always have a saved good working registry from myself available.

A double-click onto ot and everything again is as it was.

 

 

regards
Wolfgang

Re: CUT EXTRUDED BODY

Gears Phenom Gears Phenom
Gears Phenom

As @hawcad suggest.  the reason i asked you to do that test was to see if this error was due to someing in the user reg.  this confirms that it is.

 

if you are comfortable working in the registry then you can simple delete the hive:

HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\Version 109

we suggest exportign a backup 1st.  

 

be advised this will reset lots of things in SE that are users preferences...

 

if you are not comfortable working in the Reg please ask your IT person to do this or call yoru VAR or GTAC and ask them to assit in deleting the hive:

HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\Version 109


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7