Cancel
Showing results for 
Search instead for 
Did you mean: 

Callout properties

Experimenter
Experimenter

Hi All, I recently updates the Solid Edge to ST8, do you know if on the Callout Properties we can recovery the Saved settings used in the last version?

 

regards

21 REPLIES 21

Betreff: Callout properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,



it sounds as You have not changed the directory for "Report".txt file form templates in the Solid Edge installation directory to a customized folder.

 

So if You used the c:\program\Solid Edge\template\reports folder and uninstalled SE from there, I think that the only way to get Your saved callouts is to open old drafts, where they were used and save them again.

 

But before doing so, change the reports directory to a plate at Your server (as it should be for all of customized files) to keep them for future use.

 

 

regards
Wolfgang

Re: Callout properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Custom callouts are usually in Program Files\Solid Edge STX\template\reports\draftcallout.txt but could be anywhere you are pointing to templates. So, if you can retrieve your old draftcallout.txt file you should be able to use it by putting it in your current templat\reports folder.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: Callout properties

Experimenter
Experimenter

Thanks a lot, regards

Betreff: Callout properties

Genius
Genius

Hi Guys.

 

We have just changed servers and now lost our settings.

 

As you say the 'Reports' is looking at the wrong location.

 

How do we change the Reports location?

In the Solid Edge Options we cannot modify the location.

 

Kind regards

 

Darren

Betreff: Callout properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Dazzie

 

 

 

just go to the Solid Edge Options and look under the File Locations where the Reports Folder is defined.

 

20180726_1109.png

regards
Wolfgang

Betreff: Callout properties

Genius
Genius

Hi Wolfgang.

 

I know about the file locations.

 

What I am saying is that I cannot change the file location.

 

How do I get write access to be able to change it?

 

Kind regards

 

Darren.

Betreff: Callout properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Dazzie

 

 

OK, this is a matter of Your system admin.

If You are not allowed to change this or any other value, then it might be that the  Solid Edge Admin Options is in use and they defined a not access right for the users.

 

So then You have to talk to them to either change this entry too or to allow You changing it Yourselves.

 

 

regards
Wolfgang

Betreff: Callout properties

Genius
Genius

Hi Wolfgang.

 

I though I had admin rights, I am able to change some settings like the Solid Edge Admin location.

 

How can I tell if I do have admin rights?

 

Kind regards

 

Darren.

 

 

Highlighted

Betreff: Callout properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Dazzie

 

 

so then I woul dsuggest to use the SEadmin.exe tool (must be copied extra to the SE folder) to change the settings there.

 

I must say that I'm also a little bit confused that this value should not be editable by default.

 

regards
Wolfgang