Cancel
Showing results for 
Search instead for 
Did you mean: 

Callout threaded hole with countersink

Genius
Genius

Hi All.

 

I have a tapped hole with countersink.

Is there a way of adding the diameter of the countersink using callout?

 

Please see attached image

6 REPLIES 6

Re: Callout threaded hole with countersink

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Seems like it's a compound hole. Not just a threaded countersink hole but an addition of a counterbore feature. How did you add the counterbore? Or did you do a c'bore hole then chamfer the edge for the countersink?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Callout threaded hole with countersink

Genius
Genius

Hi Bshand.

 

At the moment the diameter is entered manually.

The hole is created through the hole options menu.  We have a series of holes for different diameters.

 

I have attached an image of the hole options.

Re: Callout threaded hole with countersink

Gears Phenom Gears Phenom
Gears Phenom

Hi @Dazzie,

 

What I wouls suggest is to play with the codes :

 

callouts.png

 

regards,

Arek

Re: Callout threaded hole with countersink

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I suspect it's because that "countersink" is actually a chamfer and for whatever reason doesn't register in the feature callout code.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Callout threaded hole with countersink

Genius
Genius

Hi

 

%SS does the diameter

%SA does the angle

 

But doesn't work.

Re: Callout threaded hole with countersink

Genius
Genius

Hi.

 

If I use %O1 (Start Chamfer Offset) %G1 (Start Chamfer Angle).

 

Give me dimension but not what I want.

 

I want included angle and the diameter.