Cancel
Showing results for 
Search instead for 
Did you mean: 

Callout with Configuration Name

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello Edgers:

  

A new macro for placing a callout with the Configuration name as text is attached with this message.

A single drawing view should be pre-selected when executing the macro.

 

CalloutConfig.jpg

  

This places a callout in the top right corner of the view with the config name.

You can select the callout and add a leader and/or a break line + adjust any other property.

    

The macro does not check if the drawing view is really an assembly DV.

So for a Part/Sheet Metal drawing view, it does nothing.

Also, it may appear doing nothing for an assembly DV if the configuration is 'No Selection'.

     

Requests for changes to the macro behavior are welcome.

 

 

This macro shared earlier simply displays the config name in a message box.

  

~Tushar

4 REPLIES

Re: Callout with Configuration Name

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Thank you my friend.....this will be a big help.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Callout with Configuration Name

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Glad to know it would be helpful Sean.

  

~Tushar

Re: Callout with Configuration Name

Gears Phenom Gears Phenom
Gears Phenom

My Friend,

 

It works well with ST9 beta!

 

Thanks for your effort! A huge like!

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Callout with Configuration Name

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Thanks @Imics for confirming the same.

Glad to know the macro is future ready !

 

~Tushar