Cancel
Showing results for 
Search instead for 
Did you mean: 

Cam Drawing??

Valued Contributor
Valued Contributor

Good morning
I have a lot of questions ... ^^

Not different
I'm trying to draw cam ..
What I want is to follow the path of the rectangle as if the circle had been swept.
By the way...
A rectangle is strange in shape. I can not express.

How do I do a rectangle like a circular sweep?

cam1.png

Sweep into a circle on the picture above

 

The figure below is a rectangle sweep.

cam2.png

Rectangular shape is strange.
It does not seem to follow the line like a circle.

 

We want to implement the following shape.
I used the normal cutout below, but this is not the shape! Taper created.

111.png

Can not you implement this shape in a sweep?
What other ways are there? 

 

file Attach

9 REPLIES 9

Re: Cam Drawing??

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Look in the Help for Solid Sweep. Newer command for exactly what you are trying to do.


Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Cam Drawing??

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello,

unfortunately Solid Sweep is not able to create this kind of feature.

There are already existing PRs (8954376 or 8853905) for this functionality.

 

Ota

Re: Cam Drawing??

Valued Contributor
Valued Contributor

Good morning.
Thank you for answer.
It is surprising that it can not be relatively simple.
In Gtac, I'd like to prioritize and modify the basic functions.
It's basic ...

Re: Cam Drawing??

Gears Phenom Gears Phenom
Gears Phenom
Did you try to assign an Axis of rotation during the swept ?

Re: Cam Drawing??

Valued Contributor
Valued Contributor

no.
I tried to use it after creating a path with a warp sketch.
Do you need to rotate? ..

Re: Cam Drawing??

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

the only way to get it as You want it is - at the moment - to use a swept cutout, but with multiple cross sections.

So You can tell SE to "rotate" the same cross section arround the center axis and to keep the cross section area as it should be.

 

@egarding o the other hint with using an axis for this swept cutout, this should be what we want, but it also doesn't work at them moment.

 

I knwo that it worked in the past and we could create such features exactly with that option turned on, but anyway it will not do its job at the moment (ST10 MP1)

 

 

regards
Wolfgang

Re: Cam Drawing??

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And here is a picture of what I mentioned before:

20171020_1324.PNG

regards
Wolfgang

Re: Cam Drawing??

Gears Phenom Gears Phenom
Gears Phenom

@hawcad wrote:

Hi @Hclee

  

I knwo that it worked in the past and we could create such features exactly with that option turned on, but anyway it will not do its job at the moment (ST10 MP1)

 


I was not aware about this regression.

Will it be fixed soon ?

Re: Cam Drawing??

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Fiorini

 

 

I hope it as I also hope that sweep body will work soon as they should work, that means also for such CAM features

 

regards
Wolfgang