Cancel
Showing results for 
Search instead for 
Did you mean: 

Cam Express not compatible with ST8

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Can ST8 files open in Cam Express 8.5?

 

One of the customer use ST7 before, then they upgrade to ST8.

 

After that their CAM Express 8.5 can not use.

 

See the error message as below. Any ideas?

 

Is it because of the ST8 system not compatible with CAM Express or any setting need to setup.

1 REPLY

Re: Cam Express not compatible with ST8

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi Arisy,

 

See my response over in the other message thread where you posed the same question.

 

http://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Camworks-or-Cam-Express/m-p/309972