Cancel
Showing results for 
Search instead for 
Did you mean: 

Can I convert st7 drawings to st6 compatible files

Creator
Creator

I use st6 on my laptop and st7 on my PC. Cannot upgrade the laptop to 64 bit St7 will not load.. Is there a solution. Have quite a number of drawing done on st7 I only use the laptop when I travel. Need a solution to my proble for an up coming trip!

Bill

1 REPLY

Re: Can I convert st7 drawings to st6 compatible files

You can NOT open ST7 in ST6. 

 

You could Save ST7 draft as DXF and open it in ST6  but that would only be a good solution if you need to only view the draft and maybe take some additional dimension of the 2D. 

 

You couldn't do any "work" on this and then save these edits back into ST7.

 

Are you saying that your laptop is 32 bit OS?  if so, I recomend upgrading that to 64bit.  I have to imagine that Windows EULA has a clause to allow 32bit to 64bit upgrade???

 

http://windows.microsoft.com/en-us/windows/32-bit-and-64-bit-windows#1TC=windows-7