Cancel
Showing results for 
Search instead for 
Did you mean: 

Can I install ST6 university version on Windows 7 Starter??

Experimenter
Experimenter

the system information of my computer is:

 

Windows 7 starter

Intel Atom 1.8GHz

RAM 2.00GB

OS 32 bits

 

I allready installed, but I can not work in there.

 

this is what I see

2 REPLIES 2

PStrikethrougher the System Requirements from the SE READ...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

PStrikethrougher the System Requirements from the SE README file, NO.

 

Solid Edge ST6 System Requirements and Information

Operating System Requirements and Information

This release of Solid Edge has been certified to run on the following:

  • Windows 7 Enterprise, Ultimate, or Professional (32-bit or 64-bit) with Service Pack 1
  • Windows 8 Pro or Enterprise (32-bit or 64-bit)
    • Windows 8 (home) and Windows 8 RT are not supported
  • Internet Explorer10  (IE 8 meets minimum requirements)

Solid Edge stops certifying new releases against an operating system shortly after Microsoft drops mainstream support for it. Microsoft dropped mainstream support for XP in April 2009. Microsoft dropped mainstream support for Vista in April 2012. Solid Edge ST6 will not install on Windows Vista or Windows XP.

Hardware System Requirements

Recommended system configuration

  • 64-bit (x64) processor
  • Windows 7 operating system
  • 8 GB RAM or more
  • True Color (32-bit) or 16 million colors (24-bit)
  • Screen Resolution: 1280 x 1024 or higher, widescreen format

Minimum system configuration

  • 32-bit (x86) or 64-bit (x64) processor
  • Any of the above operating systems
  • 2 GB RAM or more
  • 65K colors
  • Screen Resolution: 1280 x 1024 or higher


4 GB of disk space is required to install Solid Edge.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

With a .par file open go into Solid Edge Options -> View...

Siemens Phenom Siemens Phenom
Siemens Phenom

With a .par file open go into Solid Edge Options -> View and set Application Display to Backing store.