Cancel
Showing results for 
Search instead for 
Did you mean: 

Can ST4 files work in Student Edition?

N/A

Hello all,

I designed components using Solid Edge ST4 (.par and .asm) so can I open those files in Student Edition?

Khaled Hasan

4 REPLIES

Re: Can ST4 files work in Student Edition?

Esteemed Contributor
Esteemed Contributor
I'm pretty sure the answer is YES, but remember, once you save those files, from then on, they are in Student Edition format.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Can ST4 files work in Student Edition?

N/A
Thank you and glad u warned me about that point

Re: Can ST4 files work in Student Edition?

N/A
can you open a student edition format in st4?and would it be converted to st4 format also?

Re: Can ST4 files work in Student Edition?

Esteemed Contributor
Esteemed Contributor
can you open a student edition format in st4?and would it be converted to st4 format also?



Hi there,

No....once they are created, or saved in Student Edition, they are pretty much locked there in that format, and cannot be opened in the commercial version of Solid Edge. As it says in the startup splash screen...in red.




The only way to do this, is to export it as a neutral format, such as.....




3D models = Parasolid / 3D-PDF, etc...




2D draft files = DWG / DXF / IGES / PDF...

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000