Cancel
Showing results for 
Search instead for 
Did you mean: 

Can Solid Edge ST4 and ST6 run on Windows Server 2012 R2 64 bit

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Can Solid Edge ST4 and ST6 run on Windows Server 2012 R2 64 bit

 

Thank you and Best regards

 

Kamol T. 

1 REPLY 1

Re: Can Solid Edge ST4 and ST6 run on Windows Server 2012 R2 64 bit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Probably.  Not a supported operating system and guessing not a commonly done thing, so you just need to try it.  I run ST9 on Server 2012 and previously ran ST6 on it.  It is not the R2 version though...



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com