Can a user "Pack" components in the path finder?

Phenom
Phenom

I am working with a large assembly that consists of several large weldments. Inside the weldments I utilize the same components (stiffeners) quite frequently. In one assembly I really only have 3 different part files but they are used in over 10 different occurances/instances (quantity of ~30 entries on the path finder). The path finder displays each occurance/instance of the part.

Does SE have the ability to "pack" and "unpack" a component occurance/instance? Is this the purpose of groups?

As I start to build out my assembly I will be populating the mount flanges with all the attaching hardware (Bult+Washer+flange thickness+ Washer + Nut). There are over 90 bolted connections from one welment to another. This will create a huge assembly tree. Having the ability "pack" instances would be a nice feature.

Connection detail.pngLots of hardware.png

3 REPLIES

Re: Can a user "Pack" components in the path finder?

Esteemed Contributor
Esteemed Contributor
Groups is the only way to do this.

Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: Can a user "Pack" components in the path finder?

PLM World Member Genius PLM World Member Genius
PLM World Member Genius
Ryan

Any chance you can place connections (Bolt, washer, nuts etc..) in their respective sub-assembly?

Re: Can a user "Pack" components in the path finder?

Phenom
Phenom
Thank you Ken. That is disappointing. Maybe we should talk about defining an enhancement request for this function??

I'm going to post a follow up question and another standalone question.