Cancel
Showing results for 
Search instead for 
Did you mean: 

Can install two Dongle on the one Server machine or not?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Dear all,

 

I'm Tu, Vietnam country

I have custommer using Solid Edge floating moved from Netherlands to Vietnam (No tranfer), but now they want to buy new license Solid Edge Floating. 

My question:
1. We can install new license on the old dongle?
2. We can install 2 usb dongle on 1 server (I want to install Dongle of new license on the server machine)?
 
Thanks and Best Regard,
Tu
Best Regard,

BuiTu
2 REPLIES

Re: Can install two Dongle on the one Server machine or not?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I believe you get a new license file showing the additional license but it should still refer to the existing dongle.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Can install two Dongle on the one Server machine or not?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi Tu,
If you want to install new license in the same server you don't need to have new dongle as well. You just need to purchase new license with Siemens and load it into existing install ID. Then siemens will generate new license with your new license in it. The rest, you just need to replace the old license with the new one. Thats all.

Good luck Smiley Wink