Cancel
Showing results for 
Search instead for 
Did you mean: 

Can not display shade and references planes

Experimenter
Experimenter

My solid egde ST4 can not display shade and references planes, please help me resolve this problem.Can not display shade and reference plans.jpg

6 REPLIES 6

Re: Can not display shade and references planes

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

These settings are under the View tab of Solid Edge Options:

 

ShadeRefPlanes.png

  

Tip: You can use the Command Finder at the bottom of the Solid Edge screen to find where Solid Edge options are.

The command finder can also start found commands.

  

~Tushar Suradkar

fb.pngSolid Edge Users Facebook Group - Let's Sync

Re: Can not display shade and references planes

Experimenter
Experimenter

It is same, the problem can not reCan not display shade and reference plans2.jpgsolve. below is my option for view

Re: Can not display shade and references planes

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Your options still show reference plane shading is not checked.

Just an inch above this setting is the Application Display area;

Check OFF 'Automatic Selection' and from the pull-down list, select 'Graphics Card Driven (Advanced)'

 

Betreff: Can not display shade and references planes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Kai11

 

 

 

besides those several settings and hints mentioned by @Tushar, but what graphics card is in use?

And what's about the driver for it?

 

regards
Wolfgang

Betreff: Can not display shade and references planes

Experimenter
Experimenter

@Tushar well, it was done well. Thanks you very much. 

Betreff: Can not display shade and references planes

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Sorry I do not understand what you have written.

If the issue is resolved you can mark it a accepted solution.