Can not insert the scale value due to scale bar missing

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Inside Solid Edge drafting, I try to use scale command, but the scale bar not showing up (look picture) . Any idea?

 

 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
2 REPLIES

Re: Can not insert the scale value due to scale bar missing

Esteemed Contributor
Esteemed Contributor

Hi there,

 

From the help file....

Capture2.PNG

 

Make sure the scale ribbon bar is checked in the "customize the ribbon" selections....

Capture1.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Can not insert the scale value due to scale bar missing

Phenom
Phenom

From the attached image, it seems that the Command bar is missing.

It is hugely unlikely that it disappears just for the Scale command.

 

Can you try starting any other nearby command like Mirror or Rotate and see if the Command bar appears for those commands. In that case, see this thread where the issue was resolved.

 

~Tushar

www.SurfAndCode.in