Cancel
Showing results for 
Search instead for 
Did you mean: 

Can not set permissions borrow license on the SE ST8

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Dear all,

 

We used Solid Edge licenses borrow in ST7 is normal, but after we upgraded to version ST8 we can not set permissions license borrow for our laptop.

We only use Solid Edge when network is connect with license server.

When we disconnect network, then displays the error. mean that we do not borrow

Please help us to borrow SE license on the SE ST8

1.jpg

2.jpg

Best Regard,

BuiTu
2 REPLIES

Re: Can not set permissions borrow license on the SE ST8

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Did you install the latest ST8 license server software from the media on your license server?

LMGi
www.TLMGi.com

Re: Can not set permissions borrow license on the SE ST8

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
For License Borrowing to work, make sure this 2 things are done

1.) Use the same license file for server to user PC as well
2.) If nothing can be done, you can reset your registry of Solid Edge by going to regedit

HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge


Delete it and try again