Cancel
Showing results for 
Search instead for 
Did you mean: 

Can solid edge open the IDF file format?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello everyone,

 

Can solid edge open the IDF file format? If yes the how much compatible it is and which is the add-on for that.?

 

1 REPLY

Re: Can solid edge open the IDF file format?

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Yes, If you use PCBto3D add-on! Link

 

Here is a video from my collection how it works (well):

 

 

BR,

Imics
http://solidedgest.wordpress.com/