Can someone with ST6 or older do a simple test?

Esteemed Contributor
Esteemed Contributor

To decide a controversy here I need a simple test run on a pre-ST7 setup.

 

1. In a draft with a view which has non-Draw-in-view entities on it.

2. Do a detail with a circle that is on the view and contains those drawing entities.

3. Do the drawing entities appear in the detail view?

 

A user here claims that now those drawing entities don't appear. I claim (but don't remember) that they never did and that only DIV entities appear.

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200
6 REPLIES

Re: Can someone with ST6 or older do a simple test?

Phenom
Phenom

Even without this screen-shot there is no way non-Draw-inView entities would appear in a detail view since they do not really are part of the view.

 

dvlinesdetails.png

Re: Can someone with ST6 or older do a simple test?

Esteemed Contributor
Esteemed Contributor

That's what I thought. Thanks, Touche!

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: Can someone with ST6 or older do a simple test?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
Excellent. I hope you are going to be modest in victory. Or maybe I am too late and you are already running round the office whooping. Smiley Happy

Frank
Edinburgh University

Re: Can someone with ST6 or older do a simple test?

Esteemed Contributor
Esteemed Contributor

Smiley Happy I'm trying to remain humble  Smiley Happy

And it saves me the trouble of an IR to GTAC or our VAR.

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: Can someone with ST6 or older do a simple test?

Valued Contributor
Valued Contributor

We're currently running ST6 MP8.  I created a top view of an existing part file.  Then did a "Draw in View" and added an orange circle.  When I did a detail of that area, the detail DID actually include the circle (see pic).  I even added a line through the circle afterwards, and the detail updated with my addition.  Is that what you wanted verified?

 

Russ

 

 

Re: Can someone with ST6 or older do a simple test?

Phenom
Phenom

Russ, you have indirectly tested what was sought.

non-DIV entities won't show up in detail while DIV entities should.

 

I read-write-speak-blog in English, which is not my first language, for over 30 yrs but did not understand messages 4 and 5 or their relevance.