Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't add tolerances - ST8

Experimenter
Experimenter

I'm trying to add tolerances to my drafts, but the option seems to be grayed out. I've even tried backing up as far as the original drawings with no luck on being able to add anything, and google has failed to give me a good answer. 

 

Thanks in advance for the help!

3 REPLIES

Re: Can't add tolerances - ST8

Phenom
Phenom

Select the dimensions, click on the "X", and select the tolerance style you want and then you can enter the tolerance.

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Can't add tolerances - ST8

Experimenter
Experimenter

Thanks! I had seen that and thought it was just for changing the dimensions of the actual measurement.

Betreff: Can't add tolerances - ST8

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Casafynn

 

 

 

as mentioned by @rehenryjr You have to define what type of dimension and/or tolerance You want to have.

 

Understanding Your last answer it sounds to me as if You first define the type of dim and the tolerance before creating the dimension itself.

 

I prefer the other way.

First I create my dimensions and when I have them I consider the toleranceing aspect of the part while adding tolerances to the existing dimensions.

Toleranceing not only is a matter of dimensions but also to have GDT frames , datums, surface symbols, and much more

 

 



regards
Wolfgang