Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't dimension or modify this file imported from stl

Pioneer
Pioneer

Hi,

 

My normal approach to dealing with files that I can't edit, is to do a part copy after which the part seems to become available for modification.  That doesn't work for this file. 

 

This workaround aside, I would like to understand what is going on.  Any ideas?

2 REPLIES 2

Re: Can't dimension or modify this file imported from stl

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi @JordanMcB

I think you will find that this is a mesh model, which would explain why you can't modify it. I did an Optimize and it created a whole load of mesh bodies for the smaller text.

Re: Can't dimension or modify this file imported from stl

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JordanMcB

 

 

it is as already supposd by @Alan

 

 

in Your part file there are 17 mesh bodies, that mean not only one single mesh body, no 17 bodies.

So heer the best would be to use the new ST10 capabilities of integrated modelling (mesh and b-spline) or to run the Reverse Engineering for converting the mesh boodies back to b-rep models.

regards
Wolfgang