06-06-2014 10:03 AM - edited 06-06-2014 10:06 AM
Hello.
I have a small problem. I'm unable to see the command bar (see attachment). It doesn't appear when i click for example extrude in part mode so i can alter the parameters or a dimension line in drawing.I tryed on all aplications: part, assembly, drawing. I can't find it.
Is the an button or something so i can activate it?
I'm using ST3.
Solved! Go to Solution.
06-06-2014 01:22 PM
you can try to have anohter user log into the pc with their windows login... then test. we would assume SE would work "normal" as expected. IF this is the case then we confirm that your user regisry has somehow corrupted.
You can delete the SE user registry and next time you launch Solid Edge logged into the PC as yourself SE will rebuild your USer registry adn this should fix your issue.
much caution should be taken when working in the registry, You can hose up your entire system...
If you do not know how to do this please work with your VAR or GTAC to do so safely
06-17-2014 10:19 AM
02-03-2016 03:02 AM
Hello sir,
I am having the same problem for st6, I also followed the procedure of deleting registry, but it didnt worked out. Please suggest me some other method.
Thanks and Regards,
Ashish Sarode
02-03-2016 05:18 AM - edited 02-03-2016 05:20 AM
With Solid Edge closed, delete the following registry entry:
"HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge"
Restarting Solid Edge will then recreate this registry key and reset all the user preferences.
02-03-2016 05:46 AM
02-03-2016 06:00 AM
Deleting the registry should resolve your issue, so either you didn't delete the correct registry entry or you have something else going on.
With that said try doing the below steps, with Solid Edge closed:
In the registry, delete "HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge".
In Windows Explorer, delete "%APPDATA%\Unigraphics Solutions" and everything under it.
02-03-2016 06:02 AM
Hi there @iashishsarode1,
It is important to this process that Solid Edge is "closed" prior to, and during, the deleting of the registry key.....is that the case for you?
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000