Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Can't find coordinate system when using Part Copy.

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Yes, that is one method.

Another way of looking at it is to move the imported parasolid body to the CoordSys using the Steering Wheel.

 

Re: Can't find coordinate system when using Part Copy.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Kjetil

 

 

 

just use the Synchronous capabilities of SE, select the complete geometry, position Your steering wheel on the corresponding point and move it to the origin of the CS

 

regards
Wolfgang