Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't find keypoints in assembly sketches

Experimenter
Experimenter

As previously stated, things like circles wont highlight when i try to sketch in an assembly, when sketching on a separate part it works.

Here is what it looks like: http://imgur.com/5olSauT

And here is what i need it to look like: http://imgur.com/uULn3c6

Basically i need to make som measurements between two points but I cant make them accurate if i cant get a hold of the circle.

 

Help would be very much appreciated

2 REPLIES 2

Re: Can't find keypoints in assembly sketches

Genius
Genius

Two possbilities:

 

First, when in a Sketch in Assembly make sure Peers (peer edges).  By defualt this is off and looks like this:

Peer Edges.png

 

Otherwise, is the assembly a Family of Assemblies?  If so, keypoints will not work when making assembly features.  You would need to populate the individual family member or insert the assembly into another assembly to use Assembly Features properly.

Brian Fritz
Solid Edge Certified Professional
Solid Edge 2019 latest MP

Re: Can't find keypoints in assembly sketches

Honored Contributor
Honored Contributor

I frequently find myself making sketches to take a measurement. Typically because I need a silhouette edge on one side, and a tangent edge on the other end of the measurement.