Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't pattern mirror curves or surfaces in Part edit

Valued Contributor
Valued Contributor

Hi,

 

I use the Pattern/Mirror command frequently in Part edit with solid bodies.  Is it possible to mirror curves or surfaces using this commmand or is there a different way?

 

Thanks

11 REPLIES

Betreff: Can't pattern mirror curves or surfaces in Part edit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Planker81

 

 

 

Yes, I jsut did it again.

Creating a surface and mirrored it about a base plane

 

20180301_1721.PNG

regards
Wolfgang

Betreff: Can't pattern mirror curves or surfaces in Part edit

Valued Contributor
Valued Contributor

Does it need to be in Ordered environment?

When I'm in Synchronous, the Pattern/Mirror button is greyed out when I select a surface or curve.

Betreff: Can't pattern mirror curves or surfaces in Part edit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Planker81

 

 

no, it even is easier in sync, but I had opend the example file for another thread (pink lines) and just used this part for further explaining.

 

regards
Wolfgang

Betreff: Can't pattern mirror curves or surfaces in Part edit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Planker81

 

 

see sync mirror of surface

 

20180301_1731.PNG

regards
Wolfgang

Betreff: Can't pattern mirror curves or surfaces in Part edit

Valued Contributor
Valued Contributor

Still no luck here, I've tried a curve and a surface. The pattern/mirror button is still greyed out.

 

Betreff: Can't pattern mirror curves or surfaces in Part edit

Valued Contributor
Valued Contributor

1.PNG2.PNG

Betreff: Can't pattern mirror curves or surfaces in Part edit

Gears Phenom Gears Phenom
Gears Phenom

@Planker81  Looks like you are running ST7  can you confirm.   I assume @hawcad is on ST9 or even ST10

 

maybe this was an enhancement since ST7?

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Betreff: Can't pattern mirror curves or surfaces in Part edit

Valued Contributor
Valued Contributor

Yes, I'm on ST7

Thanks, that may explain it.

Betreff: Can't pattern mirror curves or surfaces in Part edit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Johnson_BigMatt

Hi @Planker81

 

 

but I believe to remember that I have patterned/mirrored surfaces and curves 10 or more years ago, so to say with v20 or even older.

 

Maybe I miss something but patterning of surfaces was an example with v12 or v14 presentations (handmixer, vase etc.)

 

 

regards
Wolfgang