Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't save to PDF

Not applicable
After previously using Solid Edge 3D at work I have now started using the free 2D software. Only issue being it won't allow me to save as PDF. I have a PDF printer so I can do it that way but I would rather save as pdf to keep it simple. Will this be fixed or is the pdf printer my only option?
3 REPLIES

Re: Can't save to PDF

Not applicable
Safe as PDF is not available in the Free 2D Drafting software.
Regards,
Rick B.

Re: Can't save to PDF

Not applicable
After previously using Solid Edge 3D at work I have now started using the free 2D software. Only issue being it won't allow me to save as PDF. I have a PDF printer so I can do it that way but I would rather save as pdf to keep it simple. Will this be fixed or is the pdf printer my only option?

The best thing to do is to install a print-to-PDF utility. There are a number of free ones out there; I have been using PrimoPDF for some time now with good results. The utility will typically install as a printer option in your list of printers. This way you can print anything to a PDF file.

Re: Can't save to PDF

Not applicable
I've been using doPDFv7 which works well, but native support would be nice.