Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't upload video

Honored Contributor
Honored Contributor

What is the trick to posting Video? Every time I try it give me an error saying wrong file type. I know the file type is correct.

 

My reseller will not help me with this. This was The responce form the reseller:

 

"After doing some digging I found that that falls under the website itself and that unfortunately Siemens support doesn’t have anyone that works on that so you will have to try posting the question on there and asking for assistance from them. Sorry about that"

 

30 REPLIES

Re: Can't upload video

MLombard
Retired

I'm looking into this. Can you give some additional details, such as size, type of video?

Retired Community Manager for Solid Edge. This account is no longer active.

Re: Can't upload video

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Easiest way, is create a YouTube account, upload at desired level of public visibility, then when posting a video here, select "From the Web" tab & past the YouTube link....

 

SE_Community_PostingVideoContent.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Can't upload video

MLombard
Retired

The Youtube method is what I normally do, but I tried to just upload an avi and an mp4, and neither worked. I've got both types of file already uploaded, but I couldn't do it again. So something is different from normal.

Retired Community Manager for Solid Edge. This account is no longer active.

Re: Can't upload video

Honored Contributor
Honored Contributor

Attempting to upload small file

 

File=movie_1.wmv

1.04 mb

 This time I get a new error for the first time. I don't have permission to load the file. It's a local to my computer issue.

 

Now my questions become.

How can I change the location where the vid is created to begin with?

 

There are still traces of the past user on my computer I don't know how to eliminate. apperantly the vids are being created in an area I'm not an admin for.

Re: Can't upload video

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

*TEST* ...upload of an ".WMV" file....(it says it's done it...)

SE_Community_VideoUploadTest_b.png

 

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

 

EDIT: Wasn't sure it had, but seems to have actually worked for me.

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Can't upload video

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Going a step back, here's a method that I found always works for me:

 

1. Use Solid Edge's Upload to YouTube command found in the bottom right corner:

 

1.png

 

2. This needs a YouTube account but the command itself accepts ANY video format FLV, MP4, WMV, MPG, etc. so you can upload virtually any video even if not recorded using Solid Edge.

 

In the Browse file dialog, type *.* for the file name, press <Enter>:

 

2.png

 

3. Also check ON the box for Copy Video URL to clipboard:

 

3.png

 

4. All types of videos are uploaded as MP4 to YouTube and the file size is reduced too.

 

5. Now that the URL is copied to clipboard, switch to this PLM forum and simply paste it into the 'From the Web" tab:

 

4.png

(Note: Image courtesy of SeanCresswell Smiley Wink - well actually borrowed from)

 

Regards,

 

~Tushar Suradkar

http://www.cadvertex.com

 

Re: Can't upload video

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is of course, another free method [pre video capture directly from Solid Edge]... "JING" from Techsmith http://www.techsmith.com/jing.html, and just paste the video link in amongst the text

http://screencast.com/t/w4t3aC5CKS2V ...<<here.  Robot Happy

 

Thanks for the plug too @Tushar Robot Happy

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Can't upload video

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

The Techsmith + Screencast method is foolproof, but long forgotten.

I could see it being used frequemtly on this forum until January this year.

Not many sightings after that.

 

Referring to 12GAGE's comment "I don't have permission to load the file." puzzles me in that the video could be stored at the Unigrpahics's roaming profile location, why it cannot be accesed ?

 

~Tushar

 

Re: Can't upload video

Honored Contributor
Honored Contributor

How can I edit where the built in movie recordor stores files?

 

I believe this is the root of my problem.